Select one or more webinars of interest, then submit registration form.
April 26, 2022 | 11:00 a.m. CEST
The aerospace and defense industry is racing to develop new systems and capabilities. A key to achieving faster, lower-cost development is a Model-based Engineering (MBSE) approach, integrating data through models and predicting performance through ‘digital twin’ architectures. In this session, we will discuss how Keysight’s PathWave System Design software connects to and enables your MBSE flow. It also covers how critical it is to link simulation and measurements to achieve these goals.
May 25, 2022 | 11:00 a.m. CEST
Radar coverage is the general term for the space boundary within which a radar meets the mission requirements. They depend on the type of radar and can be described in terms of detection (Pd) and false-alarm (Pfa) probabilities. A coverage map is the graphical representation of the radar coverage. In this session, we will discuss a methodology that includes the RF circuit design and signal processing effects in the calculation of the coverage map.
June 21, 2022 | 11:00 a.m. CEST
Phased array is an enabling technology for Defense and SatCom applications. The IC market is exploding with new phased array IC solutions and choosing the right Digital Beamformer IC (BFIC) is crucial for the complete system performance.
September 20, 2022 | 11:00 a.m. CEST
With satellite competition growing exponentially, advanced virtual prototyping and design platform techniques are needed to keep pace. Design teams need to drill down into any part of a design, measure components and bring results back into the system model to simulate with higher fidelity than ever possible.